MODEL BASED DESIGN TOOLBOX [Registration Code, S32K144]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MODEL BASED DESIGN TOOLBOX [Registration Code, S32K144]

3,224件の閲覧回数
electronica2pow
Contributor III

Hello to the community,

I am owner of a S32K144 platform and i would like to download the "Model Based Design Toolbox", but when i click on the link appears a message: "There is currently no Software or Support in your account. To register a new product, enter the registrion code below." Where could i find the "Registration code" in order to download that model?

I was entering codes from the NXP package, but none of them works. 

Regards,

Jorge

タグ(2)
3 返答(返信)

2,986件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Jorge, 

Please go to this link: Model-Based Design Toolbox|NXP 

Select Download

pastedImage_2.png

If you are logged in with a valid NXP account then you should see this page:

pastedImage_3.png

Can you confirm this ?

Perhaps the link you are trying to download is broken or the re-direct might not temporary working.

Hope this helps!

Daniel

2,986件の閲覧回数
electronica2pow
Contributor III

It was really helpful and you solved my problem Daniel.

But i want to tell you that your coworkers should give a look to the Reference Manual of the Toolbox: https://www.nxp.com/docs/en/reference-manual/MBDT-User-Manual-for-S32K.pdf 

Pictures don't appear, so maybe there is an issue there.

Thanks,

Jorge

0 件の賞賛
返信

2,984件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Jorge, 

Thank you for reporting the issue. Please use this one attached. I'll inform our web admin. Anyhow, please be aware that starting with v3.0.0 we have replaced the PDF documentation with MATLAB Help.

Best regards,
Daniel

0 件の賞賛
返信