MBDT support for MPC5634M or any e200z3 core processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT support for MPC5634M or any e200z3 core processors

1,646 Views
arjunraveendran
Contributor III

Hello All,

I am working on MPC5634M MCU which has e200z3 core.

I cannot find this device in list of supported devices by Model based design toolbox.

Is it possible to use any other release of MBDT for integration with Matlab/simulink.

0 Kudos
Reply
2 Replies

1,508 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Arjun, 

We do not have support for such processor in the Model-Based Design Toolboxes. The list of supported cores and SoC is shown here: Model-Based Design Toolbox|NXP 

Supported Devices

  • S32K: 32-bit Automotive General Purpose Microcontrollers
  • MPC574xP: Ultra-Reliable MPC574xP MCU for Automotive & Industrial Safety Applications
  • MPC564xL: Ultra-Reliable Dual-Core 32-bit MCU for Automotive and Industrial Applications
  • MPC567xK: Ultra-Reliable MPC567xK MCU for Automotive & Industrial Radar Applications
  • S12ZVM: S12ZVM Mixed-Signal MCU for Automotive & Industrial Motor Control Applications
  • S12ZVMB: Mixed-Signal MCU for Automotive & Industrial Motor Control Applications
  • KV1x: Kinetis® KV1x-75 MHz,  Entry-level 3ph FOC / Sensorless Motor Control MCUs based on Arm® Cortex®-M0+
  • KV3x: Kinetis® KV3x-100–120 MHz,  Advanced 3ph FOC / Sensorless Motor Control MCUs based on Arm®Cortex®-M4
  • KV4x: Kinetis KV4x-168 MHz, High Performance Motor / Power Conversion MCUs based on Arm® Cortex®-M4
  • KV5x: Kinetis® KV5x-240 MHz, Motor Control and Power Conversion, Ethernet, MCUs based on Arm® Cortex®-M7
  • MC56F827xx: MC56F823xx and MC56F827xx Digital Signal Controllers

Unfortunately, there is nothing we can do for you in this case. Sorry!

Best regards,

Daniel

0 Kudos
Reply

1,508 Views
arjunraveendran
Contributor III

Hi Daniel,

Thank you for the clarification.

Arjun.

0 Kudos
Reply