MBDT's CAN_Rx Mailbox Limitation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT's CAN_Rx Mailbox Limitation

2,216 Views
Narudol-T
Contributor III

Hi Guy,

 

I am working with MPC5744P board which have 3 CAN Channel in Simulink.

In the "FCAN_Receive" blocks set, there are 0~63 selective Buffer.

 

Issue : I have already used all 0~63 Buffer in Channel 0, I want to use them again in Channel 1~2.

Question : Does this Buffers are independent for each CAN Channel ?

 

Request : Could you point me some explaination sheet of these question ?

 

Thank you in advanced.

Narudol T.

 

Tags (1)
0 Kudos
Reply
0 Replies