MBDT for 9s12z,cann't receive mscan message?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for 9s12z,cann't receive mscan message?

Jump to solution
1,749 Views
xuxingwen0719
Contributor II

I use MBDT to generate code, compile without error, but I can only receive the can message at the moment of power-on. The attachment is my model and code.

Hardware issues have been eliminated, handwritten code can accept information normally;

I use 9s12zcva192 ,Please help me, I will be very grateful.

Labels (1)
0 Kudos
Reply
1 Solution
1,651 Views
xuxingwen0719
Contributor II

The issue has been resolved and it is hereby ending the post. MSCAN send priority is too high and must be lower than Base System Tick Priority

View solution in original post

2 Replies
1,652 Views
xuxingwen0719
Contributor II

The issue has been resolved and it is hereby ending the post. MSCAN send priority is too high and must be lower than Base System Tick Priority

1,651 Views
Daniel_Popa
NXP Employee
NXP Employee

Thank you for letting us and everyone else know the fix to this problem.

Best regards,

Daniel

0 Kudos
Reply