MBDT for 9s12z,cann't receive mscan message?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT for 9s12z,cann't receive mscan message?

跳至解决方案
1,622 次查看
xuxingwen0719
Contributor II

I use MBDT to generate code, compile without error, but I can only receive the can message at the moment of power-on. The attachment is my model and code.

Hardware issues have been eliminated, handwritten code can accept information normally;

I use 9s12zcva192 ,Please help me, I will be very grateful.

标签 (1)
0 项奖励
回复
1 解答
1,524 次查看
xuxingwen0719
Contributor II

The issue has been resolved and it is hereby ending the post. MSCAN send priority is too high and must be lower than Base System Tick Priority

在原帖中查看解决方案

2 回复数
1,525 次查看
xuxingwen0719
Contributor II

The issue has been resolved and it is hereby ending the post. MSCAN send priority is too high and must be lower than Base System Tick Priority

1,524 次查看
Daniel_Popa
NXP Employee
NXP Employee

Thank you for letting us and everyone else know the fix to this problem.

Best regards,

Daniel

0 项奖励
回复