License needed for MBDT HCP for S32G3 Board in the version 1.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License needed for MBDT HCP for S32G3 Board in the version 1.3.0

Jump to solution
623 Views
monchito911
Contributor II

Hello,

i have a doubt regarding the license needed for the MBDT for Matlab.

On the download page when i click on licenses for the MBDT HCP for the S32G board there is no license available for the 1.3.0 version. Only for the 1.2.0 version. 

Does this work for both?

Thank you for your help in advance.

0 Kudos
Reply
1 Solution
601 Views
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

View solution in original post

0 Kudos
Reply
1 Reply
602 Views
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

0 Kudos
Reply