License needed for MBDT HCP for S32G3 Board in the version 1.3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

License needed for MBDT HCP for S32G3 Board in the version 1.3.0

跳至解决方案
590 次查看
monchito911
Contributor II

Hello,

i have a doubt regarding the license needed for the MBDT for Matlab.

On the download page when i click on licenses for the MBDT HCP for the S32G board there is no license available for the 1.3.0 version. Only for the 1.2.0 version. 

Does this work for both?

Thank you for your help in advance.

0 项奖励
回复
1 解答
568 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
1 回复
569 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

0 项奖励
回复