License needed for MBDT HCP for S32G3 Board in the version 1.3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License needed for MBDT HCP for S32G3 Board in the version 1.3.0

ソリューションへジャンプ
741件の閲覧回数
monchito911
Contributor II

Hello,

i have a doubt regarding the license needed for the MBDT for Matlab.

On the download page when i click on licenses for the MBDT HCP for the S32G board there is no license available for the 1.3.0 version. Only for the 1.2.0 version. 

Does this work for both?

Thank you for your help in advance.

0 件の賞賛
返信
1 解決策
719件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
720件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @monchito911,

If the generated license is valid, it also works for the newer version of the toolbox. A single MBDT license associated with a single machine can be generated for each NXP account. Only if you change your computer you should return and generate another license for the new computer, but as long as you use the same computer, the generated license should work.

 

Best regards,

Dragos

0 件の賞賛
返信