License Error: -5, Motor Control Toolbox License Invalid,

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License Error: -5, Motor Control Toolbox License Invalid,

3,092件の閲覧回数
leo_wu
Contributor I

Hello NXP team,

I'm using model base design for DSC 56F82xxx, I have installed license and information as below

#Model-Based Design Toolbox for MATLAB/Simulink - Motor Control Toolbox for #MATLAB/Simulink MBD for DSC for Leo Wu Software Account # License for DISK_SERIAL_NUM=34d1f57c INCREMENT MC_Toolbox_DSC freescale 1.00 permanent uncounted \ VENDOR_STRING="Motor Control Toolbox for MATLAB/Simulink MBD \ for DSC" HOSTID=DISK_SERIAL_NUM=34d1f57c ISSUER="Freescale \ Semiconductor" ISSUED=02-apr-2019 ck=222 SN="FSL - 26342207" \ TS_OK SIGN="1C17 B0E3 8036 893A DC96 6722 995A CBFF CAA6 2D38 \ 9EF9 5761 FFCA 1825 1FDF 1767 7A8B 15DF C3BE BBB4 336F D38D \ 68D8 5A95 BFBD FC87 4840 BD51 1A41 124E"

pastedImage_2.png

I put license file to C:\MCToolbox\mctbx_56f82\lic, when I run the build model, will show license error as below picture:

pastedImage_1.png

How can I fix this issue? I already reset the Set Path and reinstall the MC toolbox.

I see some information when I key vol on MATLAB:

Motor Control Development Toolbox for 56F82XXX        Version 1.0        (R2012a-R2013b)

My MATLAB is R2015a, is my MATLAB doesn't support Motor Control Development Toolbox for 56F82XXX?

Thanks,

Best Regards,

Leo

0 件の賞賛
返信
4 返答(返信)

2,942件の閲覧回数
leo_wu
Contributor I

Hi NXP team

do you have any idea for this issue? Now I can run Kinetis V and S32K MBDt, But DSC still can't run because license issue -5.... thank you 

0 件の賞賛
返信

2,942件の閲覧回数
leo_wu
Contributor I

Hi Marius,

Do you have any ideas for this issue? does 56F82xx model design tools can't run on MATLAB2015a?

0 件の賞賛
返信

2,942件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

For me the toolbox worked by copying the license to the DSC\src\lic but under development the path might be different. Please try in the following locations: C:\MCToolbox\mctbx_56f82\lic or C:\MCToolbox\lic but the most important is that the license extension must be changed to .lic. Probably it will not work with .dat file extension. 

Best Regards, 

Marius

 

0 件の賞賛
返信

2,942件の閲覧回数
leo_wu
Contributor I

Hi Marius,

I have put license to C:\MCtoolbox\mctbx_56f82\lic as below :

pastedImage_1.png

but still can't use, as below picture

pastedImage_1.png

do you have any ideas?

Thanks,

Best Regards,

0 件の賞賛
返信