Import of Simulink created Project to S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import of Simulink created Project to S32DS

919件の閲覧回数
nithin-jaikar
Contributor I

Currently working with the S32K144 EVB and utilizing MATLAB Model-Based Design (MBD) for code generation, issues are being encountered while trying to import the generated project into S32 Design Studio. Despite following all instructions and references from NXP community forums and official documentation, the project fails to import into the development environment. Other manually created projects can be successfully built, imported, and deployed without any issues, but Simulink-generated projects consistently encounter this problem.

Details regarding the issue:

  • MATLAB/Simulink Version: MATLAB 2024a
  • MBD Toolbox Version: v4.2.0
  • S32 Design Studio Version: S32DS v3.5

Steps taken:

  1. Guidelines from community resources have been followed.   
  2. The generated ProjectInfo.xml file has been verified.
  3. Compatibility between the MBD Toolbox and S32 Design Studio has been checked.

A snapshot highlighting the specific point of the issue is attached for reference.

0 件の賞賛
返信
1 返信

406件の閲覧回数
rohit1749
Contributor III

I'm also facing same issue while importing xml file to s32ds. I'm using S32DS version 3.5 and MATLAB R2021b.

Someone please help me with this

0 件の賞賛
返信