IMXRT1010XXX evaluation board programming issue with MATLAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1010XXX evaluation board programming issue with MATLAB

16,035件の閲覧回数
venkatm
Contributor II

Hello Community

I am using IMXRT1010XXX evaluation board and programmed using Matlab code generation, while flashing the program to the evaluation board it is always asking for rest, when I reset the board, then the programme is not flashing to the board, the same board when i flash using mcuExpresso IDE , it is working with out any issue, Can any one faced similar issue with MATLAB?

 

Best Regards

Venkat

0 件の賞賛
返信
23 返答(返信)

1,914件の閲覧回数
venkatm
Contributor II

With MCUExpresso IDE I can able to flash the board, I could not able to flash the board using matlab support package.

 

BR

Venkat

0 件の賞賛
返信

2,013件の閲覧回数
ramprakash09
Contributor II

Hi,

Ensure that your MATLAB environment is set up correctly for the IMXRT1010XXX board. This includes having the correct toolboxes and support packages installed.

It's possible that there might be a compatibility issue between MATLAB and the IMXRT1010XXX board. If this is the case, you might need to update your MATLAB software or the board's firmware.

Regards

0 件の賞賛
返信

1,980件の閲覧回数
venkatm
Contributor II

I am using the correct support package and the board related example, still the issue occurring.

0 件の賞賛
返信