IMXRT1010XXX evaluation board programming issue with MATLAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1010XXX evaluation board programming issue with MATLAB

15,986 Views
venkatm
Contributor II

Hello Community

I am using IMXRT1010XXX evaluation board and programmed using Matlab code generation, while flashing the program to the evaluation board it is always asking for rest, when I reset the board, then the programme is not flashing to the board, the same board when i flash using mcuExpresso IDE , it is working with out any issue, Can any one faced similar issue with MATLAB?

 

Best Regards

Venkat

0 Kudos
Reply
23 Replies

1,904 Views
venkatm
Contributor II

With MCUExpresso IDE I can able to flash the board, I could not able to flash the board using matlab support package.

 

BR

Venkat

0 Kudos
Reply

2,003 Views
ramprakash09
Contributor II

Hi,

Ensure that your MATLAB environment is set up correctly for the IMXRT1010XXX board. This includes having the correct toolboxes and support packages installed.

It's possible that there might be a compatibility issue between MATLAB and the IMXRT1010XXX board. If this is the case, you might need to update your MATLAB software or the board's firmware.

Regards

0 Kudos
Reply

1,970 Views
venkatm
Contributor II

I am using the correct support package and the board related example, still the issue occurring.

0 Kudos
Reply