How do I use the Profiler Function correctly?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use the Profiler Function correctly?

Jump to solution
6,778 Views
praktikant2fs35
Contributor II

Hello,

I am using the NXP MBDT(Matalb 2017b, Toolboxversion: 4.1.0, S32K144EVB-Q100) and tried to use the Profiler Function. Attached you can find my simulink model. In that model I tried to test the Profiler Function by implementing a for-loop and measured an execution time of 3319 bus clock ticks. Then I copied the Matlab Function and expected an execution time which is twice as high. But then the FreeMASTER wasn't able to show the variable anymore it just appeared a question mark in the Variable Watch. Therefore I sent the execution time as a CAN-message using the FCAN-Send block. I measured an execution time of 187012 bus clock ticks. How is that possible? I expected a value between 6000 and 7000. Why did the FreeMASTER brake up I didn't change the configuration. Since I am already asking is it correct that the bus clock has in my model a frequency of 40MHz?

Any help on this issue would be highly appreciated!

Thanks in advance!

0 Kudos
Reply
1 Solution
6,662 Views
constantinrazva
NXP Employee
NXP Employee

To make an update here - following up the discussion in this thread MBDT blocks for measuring Idle Time or ProcessorLoad , I realized I have made some mistakes in the answer i previously gave - to correct them, we have the following:

To get the execution time, you should get the number returned by the profiler block (that has frequency of 20MHz) and divide it to this exact frequency to get the result expressed into seconds.

Execution time = profiler ticks / 20 000 000

You can also convert from profiler ticks to core ticks by multiplying this number by 4.

Core ticks = profiler ticks x 4

The period will remain the same, but now you’ll have the following:

Execution time = (profiler ticks x 4)  /  (20MHz x 4)

As you can see, as both the nominator and the denominator have been multiplied by the same constant, if you simplify this, you’ll end up with the first formula.

Kind regards,

Razvan.

View solution in original post

0 Kudos
Reply
3 Replies
6,107 Views
bcelikte
Contributor III

Hi @constantinrazva 

It is working and we are using for our models, thanks.

I mistakenly didnt't select ataomic subsystem and resuable function at packaging for another new model and I saw just the outermost's profiler result which is overall model profiler actually. Then I select atomic subsystem and reusable  for all subsytems and recalculate, this time I could see every substems' profiler but the overall execution time is increased a lot. Do you know the theory behind? Does atomic subsytem  or resuable packaging increase the execution time?

Thanks

0 Kudos
Reply
6,663 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

The clock source for the profiler is actually SPLL/4, so 20MHz. So if you want to convert from profiling cycles (LPIT cycles) to core clock cycles, you can multiply by 4 the value that you get from the profiler block.

 

If you want to convert from profiling cycles to microseconds, you can divide by value (in MHz) and then divide by 4 (because it’s 4 times slower than the core).

 

e.g.: Let’s say we have a simple function for which the profiler returns the value 22 cycles. In this scenario we have core frequency = 80MHz.

22 cycles / 80 MHz / 4 = ~0.069 us. If we’d had 112MHz core speed selected, it would have taken 22 cycles / 112MHz / 4 = ~0.049us.

 

For this example, it takes 22 * 4 = 88 CPU cycles.

Tested on your example, I got the following values:

  • 88469 profiler (PIT) bus clock ticks - for 1 subsystem (1 for loop) - 88469 / 80 / 4 = ~276us
  • 177736 profiler (PIT) bus clock ticks - for 2 subsystems (2 for loops) - 177736 / 80 / 4 = ~555.4us

What you'll have to know for using the profiler block is that in some cases you'll have to set the subsystem as an atomic unit. You can do this by right clicking the subsystem you want to profile, click on Block parameters and from there select (in the Main tab) "Treat as atomic unit" + from Code generation tab "Function packaging: Reusable function" (or nonreusable, but NOT inline). You have to do this so that you only profile code within that subsystem. These settings make sure a function is generated for the subsystem and no other code is being generated (from blocks outside that subsystem). A subsystem is just a means for users to encapsulate certain parts of models; until you set it as an atomic unit, Simulink treats it like it is just dumped into the top model (all the blocks inside). Only after this setting is done, the encapsulation takes place.

pastedImage_3.png

pastedImage_4.png

Another topic I'd like to address is FreeMASTER - you can go to the FreeMASTER configuration block and open the advanced settings. Here you'll see 3 modes available:

  • Poll-driven - here no interrupt is needed/generated - this is generally not the way you'd like to configure, as the FreeMASTER can get starved and not complete the data transfer to the PC
  • Long interrupt - all the message processing is done inside the interrupt
  • Short interrupt - the data is saved and queued inside the interrupt - this is generally the mode you'd like to select, as you should always get data out and into the PC application

If you configure the FreeMASTER like in the image below, you'd get stable connection (no '??' data). The only downside to using short interrupt is that data is not instantly transmitted to the application (but the delays are negligible).

pastedImage_5.png

Hope this helps! Please let us know if you have further issues/questions.

Kind regards,

Razvan.

6,663 Views
constantinrazva
NXP Employee
NXP Employee

To make an update here - following up the discussion in this thread MBDT blocks for measuring Idle Time or ProcessorLoad , I realized I have made some mistakes in the answer i previously gave - to correct them, we have the following:

To get the execution time, you should get the number returned by the profiler block (that has frequency of 20MHz) and divide it to this exact frequency to get the result expressed into seconds.

Execution time = profiler ticks / 20 000 000

You can also convert from profiler ticks to core ticks by multiplying this number by 4.

Core ticks = profiler ticks x 4

The period will remain the same, but now you’ll have the following:

Execution time = (profiler ticks x 4)  /  (20MHz x 4)

As you can see, as both the nominator and the denominator have been multiplied by the same constant, if you simplify this, you’ll end up with the first formula.

Kind regards,

Razvan.

0 Kudos
Reply