Freemaster with KV31: Can not detect Board information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster with KV31: Can not detect Board information

ソリューションへジャンプ
2,040件の閲覧回数
pbgemann001
Contributor III

Hello,

my setup is a KV31F120M and the Motor Control Toolbox on Matlab2019a / Windows. I have successfully compiled and downloaded a simple LED example (attached). Now I want to establish a connection to Freemaster.

I did the following:

- Add the Freemaster Data Recorder Block to the Model

- Freemaster Config -> UART1 / Baudrate: 9600

- Build

- Freemaster -> Options -> COM7 (OpenSDA) / Speed: 9600

- Start Communication leads to the ERROR: "Can not detect board Information! Communication will be paused."

Any Ideas on how to solve this issue?

タグ(2)
0 件の賞賛
返信
1 解決策
1,838件の閲覧回数
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17

元の投稿で解決策を見る

1 返信
1,839件の閲覧回数
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17