Freemaster with KV31: Can not detect Board information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freemaster with KV31: Can not detect Board information

跳至解决方案
1,523 次查看
pbgemann001
Contributor III

Hello,

my setup is a KV31F120M and the Motor Control Toolbox on Matlab2019a / Windows. I have successfully compiled and downloaded a simple LED example (attached). Now I want to establish a connection to Freemaster.

I did the following:

- Add the Freemaster Data Recorder Block to the Model

- Freemaster Config -> UART1 / Baudrate: 9600

- Build

- Freemaster -> Options -> COM7 (OpenSDA) / Speed: 9600

- Start Communication leads to the ERROR: "Can not detect board Information! Communication will be paused."

Any Ideas on how to solve this issue?

标记 (2)
0 项奖励
回复
1 解答
1,321 次查看
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17

在原帖中查看解决方案

1 回复
1,322 次查看
pbgemann001
Contributor III

Found the solution: Should be UART0 Pin: PTB16 and PTB17