Errors compiling IMXRT1xxx GPIO polling model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errors compiling IMXRT1xxx GPIO polling model

1,875件の閲覧回数
xabism
Contributor I

Hello,

I'm trying to compile a model with a GPIO input in polling mode for the MIMXRT1170-EVK and getting some errors when trying to generate the code. This model is based on the GPIO polling mode example included in the MBD Toolbox. In fact, it is the same model without the Stateflow+GPIO output part. I attached the diagnostic file and the project.

For your information, I'm using Matlab R2020b and NXP MBD Toolbox version is 1.3.

Thanks in advance.

 

 

0 件の賞賛
返信
1 返信

1,788件の閲覧回数
nxa11767
NXP Employee
NXP Employee

Hi @xabism ,

Please see this post for a fix for the problem you are seeing. What will need to do is to change the date time format in the Matlab preferences - this is explained in that post.

Hope it helps,

Alexandra

 

0 件の賞賛
返信