Errors compiling IMXRT1xxx GPIO polling model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errors compiling IMXRT1xxx GPIO polling model

1,874 Views
xabism
Contributor I

Hello,

I'm trying to compile a model with a GPIO input in polling mode for the MIMXRT1170-EVK and getting some errors when trying to generate the code. This model is based on the GPIO polling mode example included in the MBD Toolbox. In fact, it is the same model without the Stateflow+GPIO output part. I attached the diagnostic file and the project.

For your information, I'm using Matlab R2020b and NXP MBD Toolbox version is 1.3.

Thanks in advance.

 

 

0 Kudos
Reply
1 Reply

1,787 Views
nxa11767
NXP Employee
NXP Employee

Hi @xabism ,

Please see this post for a fix for the problem you are seeing. What will need to do is to change the date time format in the Matlab preferences - this is explained in that post.

Hope it helps,

Alexandra

 

0 Kudos
Reply