Error with MBDT for 9s12zvc?????

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error with MBDT for 9s12zvc?????

1,119 Views
xuxingwen0719
Contributor II
  1. I want to send more than two CAN messages, I encountered an error: MSCAN0 error Module of MSCAN0 Transmit block 'Tem_Test/CAN_Sub/CAN_Transmit' is shared with Module of another MSCAN0 Transmit block;
  2. so I follow the tutorial below to fix this bug, But when I modified the file ***MSCAN0_check.p→ ***.none, I encountered a new error, what should I do? Please help me, thank you.
  3. I use matlab 2015a
  4. pastedImage_1.png
  5. pastedImage_2.png
0 Kudos
Reply
1 Reply

1,054 Views
xuxingwen0719
Contributor II

hi community;

The problem has been found to be a solution. as follows:
1. Follow this step to repair the .c file with the following address: "https://community.nxp.com/thread/450789";
2, mbd_s12zvc_block_mscan0_check.p file can not be directly modified to .none, you need to use the following attachment to replace;

0 Kudos
Reply