Dwarf Section Corupted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dwarf Section Corupted

ソリューションへジャンプ
2,403件の閲覧回数
pbgemann001
Contributor III

Hello,

I am using a KV31F120M, MBD Toolbox and a GCC Toolchain. I can build, download and execute models on the device. I setup a connection wih Freemaster over UART as well. Whenever I try to add the .elf in options->MAPfiles I get the prompt saying: "Dwarf Section corupted". This happens no matter what project I build (Simple, Complex, Examples from the Toolbox). I assume there is something wrong with the settings of the Toolchain?

I will gladly provide any Information about my settings.

Thank you

Paul

タグ(5)
0 件の賞賛
返信
1 解決策
2,329件の閲覧回数
pbgemann001
Contributor III

Hi dumitru-daniel.popa

It looks like the solution was way less complex. I reinstalled the latest version of Freemaster and now it works fine.
Thanks for your response anyway!

Best regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,329件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌,

This toolbox was not designed from the beginning to support the GCC hence some issues might occurs.

Can you explain your procedure of trying to generate the map files ?

If it does not works by adding the arguments in the UI, then we can try to pass is directly from the *.tmf file as a direct argument to the linker.

Best regards,
Daniel

0 件の賞賛
返信
2,330件の閲覧回数
pbgemann001
Contributor III

Hi dumitru-daniel.popa

It looks like the solution was way less complex. I reinstalled the latest version of Freemaster and now it works fine.
Thanks for your response anyway!

Best regards

Paul

0 件の賞賛
返信