Delays before starting application?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Delays before starting application?

ソリューションへジャンプ
1,926件の閲覧回数
eungsoolee
Contributor II

Hi Daniel

I am waiting for your response.

And I tested the CAN module and asked another question.

Test Scenario
My board sends one message to CANoe.

Connection procedure

1. Power on my board.
2. Wait for enough time (3-5 seconds)
3.Canoe tries CAN connection.

If I do this in the order of 1, 2, 3, then my board sends a CAN message without any problems.

However, my board does not send a CAN message if I perform the sequence 3 times without giving enough time for the second sequence.

Also, after performing step 3, if I perform steps 1 and 2, my board does not send a CAN message.
(The above problem does not occur when hand coding the CAN module in the code warrior.)

Does the file created by the toolbox need enough time to perform the bootload procedure?

Or

When I create a CAN test module, is there anything I should pay attention to when initializing the CAN module?

0 件の賞賛
返信
1 解決策
1,790件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi eungsoo Lee,

Are you using Delay before start of application option ?Capture.JPG

That might explain the behavior you are seeing. This mechanism is explained in the RAppIDBL_UserManual.pdf in chapter 2.7

quote

"Eight bytes offset from a valid RCHW (see Microcontroller Reference Manual for
more information) there is a four byte field that defines the amount of time (in
microseconds) the bootloader will delay before jumping to the Application. If the
field is 0xFFFFFFFF then the delay will default to 20ms. Otherwise it will delay as
long as the user specifies in the field."

Hope this helps!

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,791件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi eungsoo Lee,

Are you using Delay before start of application option ?Capture.JPG

That might explain the behavior you are seeing. This mechanism is explained in the RAppIDBL_UserManual.pdf in chapter 2.7

quote

"Eight bytes offset from a valid RCHW (see Microcontroller Reference Manual for
more information) there is a four byte field that defines the amount of time (in
microseconds) the bootloader will delay before jumping to the Application. If the
field is 0xFFFFFFFF then the delay will default to 20ms. Otherwise it will delay as
long as the user specifies in the field."

Hope this helps!

Best regards,

Daniel

0 件の賞賛
返信