DEVKIT-MPC5744P: PWM input capture problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEVKIT-MPC5744P: PWM input capture problem

2,154 次查看
yanshimian
Contributor I

Hello:

   For the timer demo of MPC5744P MBD Toolbox: 'etimer_input_frequency_mpc574xP'.

   It works well if I do nothing modification.

   Then I only change the counter 0 input pin from PTA0 to PTD10 in the "eTimer_Config" block. It doesn't work.

   It's the same for the counter 1 and conter 2, the first pin option is OK and the second pin option is not OK.

   

    pin.JPG

freeMASTER.JPG

标记 (1)
2 回复数

2,020 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello yanshimian‌,

Have you applied the patch from this thread https://community.nxp.com/thread/499879 ?

Best Regards,

Marius

2,020 次查看
yanshimian
Contributor I

Thanks for your help, it's OK now.