CLOCK MHZ S32K312

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CLOCK MHZ S32K312

跳至解决方案
540 次查看
paul_ephraim_13
Contributor III

paul_ephraim_13_0-1729229850527.png

IN CLOCKING OPTION (UNDER HARDWARE SETTINGS ) I AM HAVING 0 MHZ , BUT I HAVE CONFIGURED IT TO S32K312 BOARD 

 

0 项奖励
回复
1 解答
476 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

The problem you are facing seems to be caused by the non-compliant setting of the configuration project. In the Hardware tab you will find the link from the Configuration Template section, make sure it points to the correct configuration project.

dragostoma_1-1729678064182.png

After you correctly set the path to the configuration project, the frequency of 120 Mhz should be displayed correctly. Let us know how the check went.

dragostoma_2-1729678093309.png

 

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
1 回复
477 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

The problem you are facing seems to be caused by the non-compliant setting of the configuration project. In the Hardware tab you will find the link from the Configuration Template section, make sure it points to the correct configuration project.

dragostoma_1-1729678064182.png

After you correctly set the path to the configuration project, the frequency of 120 Mhz should be displayed correctly. Let us know how the check went.

dragostoma_2-1729678093309.png

 

Best regards,

Dragos

0 项奖励
回复