CLOCK MHZ S32K312

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLOCK MHZ S32K312

Jump to solution
560 Views
paul_ephraim_13
Contributor III

paul_ephraim_13_0-1729229850527.png

IN CLOCKING OPTION (UNDER HARDWARE SETTINGS ) I AM HAVING 0 MHZ , BUT I HAVE CONFIGURED IT TO S32K312 BOARD 

 

0 Kudos
Reply
1 Solution
496 Views
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

The problem you are facing seems to be caused by the non-compliant setting of the configuration project. In the Hardware tab you will find the link from the Configuration Template section, make sure it points to the correct configuration project.

dragostoma_1-1729678064182.png

After you correctly set the path to the configuration project, the frequency of 120 Mhz should be displayed correctly. Let us know how the check went.

dragostoma_2-1729678093309.png

 

Best regards,

Dragos

View solution in original post

0 Kudos
Reply
1 Reply
497 Views
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

The problem you are facing seems to be caused by the non-compliant setting of the configuration project. In the Hardware tab you will find the link from the Configuration Template section, make sure it points to the correct configuration project.

dragostoma_1-1729678064182.png

After you correctly set the path to the configuration project, the frequency of 120 Mhz should be displayed correctly. Let us know how the check went.

dragostoma_2-1729678093309.png

 

Best regards,

Dragos

0 Kudos
Reply