As a slave node , the controller can't receive LIN frame from the master node. Based on s32k144 MBD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

As a slave node , the controller can't receive LIN frame from the master node. Based on s32k144 MBD

1,078件の閲覧回数
Even1
Contributor I

Hello everyone:

     I want to the controller receive the LIN frame as slave node,The master node sends the header and responds.

      I build the  simulink model of the slave node based on the 'lin_slave_s32k14x' example,the model screenshot is as follows:

Even1_0-1717661040134.pngEven1_0-1717661040134.pngEven1_1-1717661096143.pngEven1_1-1717661096143.pngEven1_2-1717661172936.pngEven1_2-1717661172936.png

After downloading the code, the master node sends the header and response, but the slave node controller does not take any action.

The attached is the ldf file and the simulink model based on matlab 2023b.

           Thank you very much!

0 件の賞賛
返信
1 返信

1,076件の閲覧回数
Even1
Contributor I

This is the attachment.

0 件の賞賛
返信