As a slave node , the controller can't receive LIN frame from the master node. Based on s32k144 MBD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

As a slave node , the controller can't receive LIN frame from the master node. Based on s32k144 MBD

487 次查看
Even1
Contributor I

Hello everyone:

     I want to the controller receive the LIN frame as slave node,The master node sends the header and responds.

      I build the  simulink model of the slave node based on the 'lin_slave_s32k14x' example,the model screenshot is as follows:

Even1_0-1717661040134.pngEven1_1-1717661096143.pngEven1_2-1717661172936.png

After downloading the code, the master node sends the header and response, but the slave node controller does not take any action.

The attached is the ldf file and the simulink model based on matlab 2023b.

           Thank you very much!

0 项奖励
回复
1 回复

485 次查看
Even1
Contributor I

This is the attachment.

0 项奖励
回复