1.2.0 RTM vs 1.4.0 RFP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

1.2.0 RTM vs 1.4.0 RFP

跳至解决方案
2,948 次查看
mweiss
Contributor II

Dear NXP Staff,

we are currently working with 1.2.0 and MATLAB/Simulink. From other forum posts we have learned about the difference of RTM (ready for manufacturing) and EAR (early access release).

Since the end of may there is 1.4.0 RFP. Does it mean "ready for production"? What is the difference to RTM?

Thx, Markus

标记 (2)
0 项奖励
回复
1 解答
2,868 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @mweiss, 

There is no difference in terms of the toolbox purpose between 1.2.0 RTM and 1.4.0 RFP, this being just an internal term that we are using for our releases. Hence, the latest MBDT for S32K3 version (released end of may) is not ready for production, but an enhanced version of the 1.2.0, which enables multiple processors of the S32K3 family, and provides several additional features and improvements on the toolbox capabilities.

Please let us know if you have any additional questions or if you encounter any issues while using MBDT for S32K3.

Thank you,

Irina

 

在原帖中查看解决方案

2 回复数
2,869 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @mweiss, 

There is no difference in terms of the toolbox purpose between 1.2.0 RTM and 1.4.0 RFP, this being just an internal term that we are using for our releases. Hence, the latest MBDT for S32K3 version (released end of may) is not ready for production, but an enhanced version of the 1.2.0, which enables multiple processors of the S32K3 family, and provides several additional features and improvements on the toolbox capabilities.

Please let us know if you have any additional questions or if you encounter any issues while using MBDT for S32K3.

Thank you,

Irina

 

2,604 次查看
mweiss
Contributor II

Created separate thread.

0 项奖励
回复