1.2.0 RTM vs 1.4.0 RFP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1.2.0 RTM vs 1.4.0 RFP

ソリューションへジャンプ
2,949件の閲覧回数
mweiss
Contributor II

Dear NXP Staff,

we are currently working with 1.2.0 and MATLAB/Simulink. From other forum posts we have learned about the difference of RTM (ready for manufacturing) and EAR (early access release).

Since the end of may there is 1.4.0 RFP. Does it mean "ready for production"? What is the difference to RTM?

Thx, Markus

タグ(2)
0 件の賞賛
返信
1 解決策
2,869件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @mweiss, 

There is no difference in terms of the toolbox purpose between 1.2.0 RTM and 1.4.0 RFP, this being just an internal term that we are using for our releases. Hence, the latest MBDT for S32K3 version (released end of may) is not ready for production, but an enhanced version of the 1.2.0, which enables multiple processors of the S32K3 family, and provides several additional features and improvements on the toolbox capabilities.

Please let us know if you have any additional questions or if you encounter any issues while using MBDT for S32K3.

Thank you,

Irina

 

元の投稿で解決策を見る

2 返答(返信)
2,870件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @mweiss, 

There is no difference in terms of the toolbox purpose between 1.2.0 RTM and 1.4.0 RFP, this being just an internal term that we are using for our releases. Hence, the latest MBDT for S32K3 version (released end of may) is not ready for production, but an enhanced version of the 1.2.0, which enables multiple processors of the S32K3 family, and provides several additional features and improvements on the toolbox capabilities.

Please let us know if you have any additional questions or if you encounter any issues while using MBDT for S32K3.

Thank you,

Irina

 

2,605件の閲覧回数
mweiss
Contributor II

Created separate thread.

0 件の賞賛
返信