mqx support on ssh

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mqx support on ssh

1,528 Views
sannyfrancis
Contributor I

Hi,

Kindly let me know of the mqx support for ssh.

Has anyone tried porting openssh on to mqx?

Thanks in advance

0 Kudos
Reply
3 Replies

1,178 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Sanny:

We have included third party Wolfssl library code for TLS protocl.

Please refer to the SSL manual

https://www.wolfssl.com/wolfSSL/Docs-wolfssl-manual-toc.html

Here you can see the patch for cyassl

Now Available: MQX 4.2.0.1 Patch

Regards

Daniel

0 Kudos
Reply

1,178 Views
sannyfrancis
Contributor I

Thanks for the quick reply......

You are talking of SSL.

I would like to know if there are any support for SSH in MQX?

1> I have come across Mocana NanoSSH.Is there any supporting login examples sources for using NanoSSH / Documentation on the same? Can this be easily integrated? Could you shed more details on Mocana NanoSSH?

2> Since we are using MQX 3.1, What other steps would be needed from my end to integrate NanoSSH?

0 Kudos
Reply

1,178 Views
DavidS
NXP Employee
NXP Employee

Hi Sanny,

Short answer is Mocana support for Kinetis was deprecated several years ago.

The WolfSSL is only SSL and currently does not support SSH.  Ping them to see if they have SSH on the roadmap.

Regards,

David

0 Kudos
Reply