mqx support on ssh

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mqx support on ssh

2,082件の閲覧回数
sannyfrancis
Contributor I

Hi,

Kindly let me know of the mqx support for ssh.

Has anyone tried porting openssh on to mqx?

Thanks in advance

0 件の賞賛
返信
3 返答(返信)

1,732件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Sanny:

We have included third party Wolfssl library code for TLS protocl.

Please refer to the SSL manual

https://www.wolfssl.com/wolfSSL/Docs-wolfssl-manual-toc.html

Here you can see the patch for cyassl

Now Available: MQX 4.2.0.1 Patch

Regards

Daniel

0 件の賞賛
返信

1,732件の閲覧回数
sannyfrancis
Contributor I

Thanks for the quick reply......

You are talking of SSL.

I would like to know if there are any support for SSH in MQX?

1> I have come across Mocana NanoSSH.Is there any supporting login examples sources for using NanoSSH / Documentation on the same? Can this be easily integrated? Could you shed more details on Mocana NanoSSH?

2> Since we are using MQX 3.1, What other steps would be needed from my end to integrate NanoSSH?

0 件の賞賛
返信

1,732件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Sanny,

Short answer is Mocana support for Kinetis was deprecated several years ago.

The WolfSSL is only SSL and currently does not support SSH.  Ping them to see if they have SSH on the roadmap.

Regards,

David

0 件の賞賛
返信