VID PID USB license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
8,932件の閲覧回数
admin
Specialist II

I'm developing on MQX an USB Host that read and save a configuration from an USB mass storage (USB device), I need to purchase VID from www.usb.org ? Can I purchase only a PID from Freescale?

 

ラベル(1)
タグ(1)
1 解決策
4,670件の閲覧回数
admin
Specialist II

Freescale, as a member of the USB-IF, owns a Vendor ID and manages a database of Product IDs to be used in association with the VID.

Customers can apply for a license to use Freescale’s VID with a uniquely assigned PID. You will need to work with your local Freescale Sales or Field Engineering team so they can request a PID on your behalf.

元の投稿で解決策を見る

6 返答(返信)
4,670件の閲覧回数
admin
Specialist II

Thanks JuroV!!!!

... so I need a VID only if I'm developing an USB device, but in this case can I use a Freescale VID and buy from Freescale only a PID ?

 

0 件の賞賛
返信
4,670件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

 

selling PIDs is prohibited by USB-IF statements. So Freescale cannot sell any PID. Freescale can only give you a PID free of charge, but we don't do that. All PIDs within Freescale's VID (0x0425, former Motorola VID) are managed by Freescale. You can use PID 0x0001 for your application. You MUST NOT use Freescale's VID for your market-targeted application- you must either purchase a VID or became an USB-IF member.

All those companies that sold PIDs in the past stopped doing this as far as I know.

0 件の賞賛
返信
4,670件の閲覧回数
larsknudsen
Contributor II

Hi,

it has been some years since your post and I was wondering if Freescale has changed policy on this as there are many other vendors who sub-license PIDs to small scale productions (<10K units/PID, I believe) for their customers.  We are making a product that is set to help many but doesn't really make any money (yet at least) - www.empirikit.com and we are using the Freedom boards with little or no modifications with our own firmware on them (of course).  We don't have $5K to hand over to USB.org for a VID (a bit expensive for small productions, IMO) and we are really in need of an official VID/PID combo for the science kit we are making.

Is there any way Freescale can help out?

br

Lars

0 件の賞賛
返信
4,671件の閲覧回数
admin
Specialist II

Freescale, as a member of the USB-IF, owns a Vendor ID and manages a database of Product IDs to be used in association with the VID.

Customers can apply for a license to use Freescale’s VID with a uniquely assigned PID. You will need to work with your local Freescale Sales or Field Engineering team so they can request a PID on your behalf.

4,670件の閲覧回数
Mickey
Contributor III

Hi

    Can I use the VID 0x0425, PID 0x0001 USB to as my product? personal sales, non-company?

0 件の賞賛
返信
4,670件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi.

 

VIDs are purchased only for device applications. If you want to developa some USB host- only application, you dont need to purchase any VIDs (what for?).

0 件の賞賛
返信