The debugger is not connected to PE device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The debugger is not connected to PE device

Jump to solution
1,652 Views
davidzhou
Contributor V

Hi,

I am a newbie on freescale. Just installed MQX and Code Worrier (Ver10.6.4.) I imported Hello and Hello2 projects. Compiled and be able to debug into the program. But the debugger crashes the _SET_KERNEL_DATA inside the call _mqx( (MQX_INITIALIZATION_STRUCT_PTR) &MQX_init_struct );

The hello2_twrk60f120m is debugged as flash_debug with Target settings as TWRK60F120M_OSJTAG.

What is wrong?

Thank you,

David

0 Kudos
Reply
1 Solution
1,526 Views
davidzhou
Contributor V

This may be caused by either no license or MQX plugin was not installed. After installed MQX plugin and with activated license key, the problem runs away.

Thanks,

View solution in original post

0 Kudos
Reply
1 Reply
1,527 Views
davidzhou
Contributor V

This may be caused by either no license or MQX plugin was not installed. After installed MQX plugin and with activated license key, the problem runs away.

Thanks,

0 Kudos
Reply