TCP/IP Out of Memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TCP/IP Out of Memory

1,440件の閲覧回数
diegoderganz
Contributor II

I'm using MQX 4.0.1 and Code Warrior 10.4

HW: M52259EVB running Int. Flash Debug

I have installed the http web server and I have a page that automaticaly update the values every 10 seconds.

In around 5-10 minutes I got "Out of Memory" in the TCP/IP Task.

Thread [ID: 0x10002] (Suspended: Signal 'Process Suspended' received. Description: Process Suspended.) 

    2 SOCK_STREAM_listen() sstream.c:526 0x0000c118 

    1 0xFF000388 (0xFF000388)()  0xff000388 

Or sometime directly "Unhandled Interrupt"

Thread [ID: 0x10002] (Suspended: Signal 'Process Suspended' received. Description: Process Suspended.)   

    2 SOCK_STREAM_listen() sstream.c:548 0x0000c1c0   

    1 0xFF000388 (0xFF000388)()  0xff000388   

What can be the problem?

Best regards,

Diego Derganz


ラベル(1)
0 件の賞賛
返信
0 返答(返信)