Source files not recompiling after they are altered when using Workbench Project->BatchBuild->Debug->Make.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Source files not recompiling after they are altered when using Workbench Project->BatchBuild->Debug->Make.

1,363 次查看
rickstuart
Contributor V

This is probably a setting deep w/in Workbench.  But I haven't found it yet.  Does anyone know of a solution to this problem I am having:

Source files not recompiling after they are altered when using Workbench Project->BatchBuild->Debug->Make.

I'm used to Workbench not working as I expect it to and usually do a BuildAll for any project I touch then do a Build&Run (GreenArrow) which does what I have come to expect (Only a link and send-to-target).

-thanks

标记 (3)
0 项奖励
回复
4 回复数

1,248 次查看
rickstuart
Contributor V

I should probably add that the source files are in other projects in the workspace that only compile to produce a library file.  And that those source files do not recompile when using Workbench Project->BatchBuild->Debug->Make.

0 项奖励
回复

1,248 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello rick:

Can you mention the IDE you use? (CodeWarrior, IAR, Keil)

This sounds like an issue with the build/make system.

Regards!

Jorge Gonzalez

0 项奖励
回复

1,248 次查看
rickstuart
Contributor V

IAR Embedded Workbench for ARM 7.20.5.7624

IAR Embedded Workbench common components 7.1.2.3324

0 项奖励
回复

1,248 次查看
DavidS
NXP Employee
NXP Employee

Hi Rick,

I've had similar issue with other IDE's when either the IDE or workspace or source code are in the C:\Program Files path on Windows 7 machines.

The path adds extra permissions that the IDE doesn't know about so after initial access to file you cannot delete or update.

This might not be your issue but wanted to share.

My solution was to uninstall and re-install to non-Program Files path.

Regards,

David

0 项奖励
回复