Shell tasks blocks other tasks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shell tasks blocks other tasks

Jump to solution
1,570 Views
simonepuschmann
Contributor II

I try to use examples with separate shell_task (like example in mqx - mfs - sdcard) and have the problem, that only the shell_task started.

The sdcard_task only started when I disable the shell_task. Must I something change in the config file to run the example correct?

Tags (2)
0 Kudos
Reply
1 Solution
1,366 Views
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

View solution in original post

0 Kudos
Reply
1 Reply
1,367 Views
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

0 Kudos
Reply