Shell tasks blocks other tasks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Shell tasks blocks other tasks

跳至解决方案
1,629 次查看
simonepuschmann
Contributor II

I try to use examples with separate shell_task (like example in mqx - mfs - sdcard) and have the problem, that only the shell_task started.

The sdcard_task only started when I disable the shell_task. Must I something change in the config file to run the example correct?

标记 (2)
0 项奖励
回复
1 解答
1,425 次查看
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,426 次查看
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

0 项奖励
回复