Shell tasks blocks other tasks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shell tasks blocks other tasks

ソリューションへジャンプ
1,562件の閲覧回数
simonepuschmann
Contributor II

I try to use examples with separate shell_task (like example in mqx - mfs - sdcard) and have the problem, that only the shell_task started.

The sdcard_task only started when I disable the shell_task. Must I something change in the config file to run the example correct?

タグ(2)
0 件の賞賛
返信
1 解決策
1,358件の閲覧回数
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,359件の閲覧回数
JerryFan
NXP Employee
NXP Employee

So the original example mfs-sdcard did not work? And which board you worked on, TWR board?

Or the example did not work after being modified? What modification you ever made?

0 件の賞賛
返信