SCI: What IO_SERIAL_RAW_IO flag is?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCI: What IO_SERIAL_RAW_IO flag is?

Jump to solution
1,592 Views
oscar
Contributor I

I know that the question is very easy, but I didn't see the difference in the MQX code

0 Kudos
Reply
1 Solution
1,406 Views
PetrL
NXP Employee
NXP Employee

As written in MQX IO manual  - No processing of I/O done. But you are right, there is no need to set this flag (and no also effect on driver fuctionality), because this is default mode for serial driver.

 

PetrL

 

View solution in original post

0 Kudos
Reply
1 Reply
1,407 Views
PetrL
NXP Employee
NXP Employee

As written in MQX IO manual  - No processing of I/O done. But you are right, there is no need to set this flag (and no also effect on driver fuctionality), because this is default mode for serial driver.

 

PetrL

 

0 Kudos
Reply