RTC and power source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTC and power source

跳至解决方案
1,095 次查看
troide
Contributor II

Hello Community,

I use RTC API in MQX 4.1 to keep the track of time in my application. Based on K60 RM, the RTC is an always powered block that is powered by the battery power supply(VBAT) but in my case it loses the track of time every time I recycle the power. I should mention that I use twr-k60f120 and I have the coin battery in the slot. Any idea what's wrong?


Cheers!

标记 (2)
0 项奖励
回复
1 解答
998 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello S M:

There is a jumper to select VBAT power (J9). Check the jumper is in position 2-3 so that VBAT can be supplied from coin battery:

TWRK60_VBAT.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
999 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello S M:

There is a jumper to select VBAT power (J9). Check the jumper is in position 2-3 so that VBAT can be supplied from coin battery:

TWRK60_VBAT.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复