RTC and power source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,746件の閲覧回数
troide
Contributor II

Hello Community,

I use RTC API in MQX 4.1 to keep the track of time in my application. Based on K60 RM, the RTC is an always powered block that is powered by the battery power supply(VBAT) but in my case it loses the track of time every time I recycle the power. I should mention that I use twr-k60f120 and I have the coin battery in the slot. Any idea what's wrong?


Cheers!

タグ(2)
0 件の賞賛
返信
1 解決策
1,649件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello S M:

There is a jumper to select VBAT power (J9). Check the jumper is in position 2-3 so that VBAT can be supplied from coin battery:

TWRK60_VBAT.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,650件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello S M:

There is a jumper to select VBAT power (J9). Check the jumper is in position 2-3 so that VBAT can be supplied from coin battery:

TWRK60_VBAT.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信