MQX with duoble ethernet interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX with duoble ethernet interface

Jump to solution
1,263 Views
MKnecht
Contributor I

Hi,

 

has anybody ever used MQX on a system with two (physical) independant

ethernet connections ? 

I need to run two IP Stacks on two ethernet Interfaces at the same time.

Each in an individual network.

 

regards

 

Michael

0 Kudos
Reply
1 Solution
936 Views
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

View solution in original post

0 Kudos
Reply
1 Reply
937 Views
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

0 Kudos
Reply