MQX with duoble ethernet interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX with duoble ethernet interface

ソリューションへジャンプ
1,748件の閲覧回数
MKnecht
Contributor I

Hi,

 

has anybody ever used MQX on a system with two (physical) independant

ethernet connections ? 

I need to run two IP Stacks on two ethernet Interfaces at the same time.

Each in an individual network.

 

regards

 

Michael

0 件の賞賛
返信
1 解決策
1,421件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,422件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

0 件の賞賛
返信