MQX with duoble ethernet interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX with duoble ethernet interface

跳至解决方案
1,739 次查看
MKnecht
Contributor I

Hi,

 

has anybody ever used MQX on a system with two (physical) independant

ethernet connections ? 

I need to run two IP Stacks on two ethernet Interfaces at the same time.

Each in an individual network.

 

regards

 

Michael

0 项奖励
回复
1 解答
1,412 次查看
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,413 次查看
DavidS
NXP Employee
NXP Employee

Hi Michael,

Our MCF54418 family of microprocessors has two Ethernets and is supported by FSLMQX.

Regards,

David

 

0 项奖励
回复