MQX dma api

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX dma api

Jump to solution
1,835 Views
Nouchi
Senior Contributor II

Hello,

I'm looking for examples or code snippets using MQX dma API (for vybrid M4 core).

Thanks,

Emmanuel

0 Kudos
Reply
1 Solution
1,493 Views
soledad
NXP Employee
NXP Employee

Hello Emmanuel,

Please check the sai_dma_demo example that is located at the below path after install MQX 4.1.

C:\Freescale\Freescale_MQX_4_1\mqx\examples\sai_dma_demo\build\ds5

This example shows the use of the DMA driven SAI driver.

Regards

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 
 

View solution in original post

0 Kudos
Reply
2 Replies
1,494 Views
soledad
NXP Employee
NXP Employee

Hello Emmanuel,

Please check the sai_dma_demo example that is located at the below path after install MQX 4.1.

C:\Freescale\Freescale_MQX_4_1\mqx\examples\sai_dma_demo\build\ds5

This example shows the use of the DMA driven SAI driver.

Regards

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 
 

0 Kudos
Reply
1,493 Views
Nouchi
Senior Contributor II

You're right, DMA API is shown in the SAI driver.

Unfortunately, the MQX 4.1 it's not available yet with Timesys environment, I tried it, but it seems to have some conflicts with DMA linux driver (UART console driver stops).

Emmanuel

0 Kudos
Reply