Custom board with MQX 4.1 on Codewarrior 10.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom board with MQX 4.1 on Codewarrior 10.5

ソリューションへジャンプ
1,644件の閲覧回数
oscargarciaabad
Contributor III

Hello,

My Name is Oscar and I'm trying to create a Project for my custom borad using MQX 4.1. I'm using codewarrior 10.5.

I clone the TWR-K60F120M (it suits to my custom board pretty well). The cloning process is done using the clone wizard from freescale (installed with MQX 4.1). There are no problems on the process itself, and after the process is done I can build the libraries with no problems. But when I want to creata a new MQX 4.1 project for my custom board, it does not appear in the list of available devices.

What I did wrong? How can I solve that?

Thanks in advances!

Oscar.

0 件の賞賛
返信
1 解決策
1,382件の閲覧回数
weapon
Senior Contributor I

Hi Oscar,

please refer to https://community.freescale.com/message/356271#356271

I think that may be helpful.

B.R

XWP

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,383件の閲覧回数
weapon
Senior Contributor I

Hi Oscar,

please refer to https://community.freescale.com/message/356271#356271

I think that may be helpful.

B.R

XWP

0 件の賞賛
返信
1,382件の閲覧回数
oscargarciaabad
Contributor III

Hi  Weiping Xu,

It worked.

Many thanks.

Oscar

0 件の賞賛
返信