MQX dma api

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,810件の閲覧回数
Nouchi
Senior Contributor II

Hello,

I'm looking for examples or code snippets using MQX dma API (for vybrid M4 core).

Thanks,

Emmanuel

0 件の賞賛
返信
1 解決策
1,468件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Emmanuel,

Please check the sai_dma_demo example that is located at the below path after install MQX 4.1.

C:\Freescale\Freescale_MQX_4_1\mqx\examples\sai_dma_demo\build\ds5

This example shows the use of the DMA driven SAI driver.

Regards

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 
 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,469件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Emmanuel,

Please check the sai_dma_demo example that is located at the below path after install MQX 4.1.

C:\Freescale\Freescale_MQX_4_1\mqx\examples\sai_dma_demo\build\ds5

This example shows the use of the DMA driven SAI driver.

Regards

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 
 

0 件の賞賛
返信
1,468件の閲覧回数
Nouchi
Senior Contributor II

You're right, DMA API is shown in the SAI driver.

Unfortunately, the MQX 4.1 it's not available yet with Timesys environment, I tried it, but it seems to have some conflicts with DMA linux driver (UART console driver stops).

Emmanuel

0 件の賞賛
返信