Just want to clarify to myself... (need your help)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Just want to clarify to myself... (need your help)

Jump to solution
1,265 Views
naftalir
Contributor III

What is the difference between esdhc and sdcard?

from the example of the sdcard with esdhc, the "esdhc" is opened first of all (so i assume this is the low-level driver) and then the SD Commands are send.

only then the "sdcard" is installed and open, and the partition manager is installed on top of it (and MFS on top of the partition manager).

Im a bit confused because i thought esdhc is the sd driver like: spi, sdhc only faster and the "sdcard" getting me confused of its goal and need.

If someone can please explain it to me i will be thankful.

Thank you.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
922 Views
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Good references:

http://en.wikipedia.org/wiki/Secure_Digital

Freescale Enhanced Secure Digital Host Controller (eSDHC)

The Enhanced Secure Digital Host Controller provides an interface

for MMC, SD, and SDIO types of memory cards.

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
923 Views
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Good references:

http://en.wikipedia.org/wiki/Secure_Digital

Freescale Enhanced Secure Digital Host Controller (eSDHC)

The Enhanced Secure Digital Host Controller provides an interface

for MMC, SD, and SDIO types of memory cards.

Regards,

David

0 Kudos
Reply