Just want to clarify to myself... (need your help)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Just want to clarify to myself... (need your help)

跳至解决方案
1,282 次查看
naftalir
Contributor III

What is the difference between esdhc and sdcard?

from the example of the sdcard with esdhc, the "esdhc" is opened first of all (so i assume this is the low-level driver) and then the SD Commands are send.

only then the "sdcard" is installed and open, and the partition manager is installed on top of it (and MFS on top of the partition manager).

Im a bit confused because i thought esdhc is the sd driver like: spi, sdhc only faster and the "sdcard" getting me confused of its goal and need.

If someone can please explain it to me i will be thankful.

Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
939 次查看
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Good references:

http://en.wikipedia.org/wiki/Secure_Digital

Freescale Enhanced Secure Digital Host Controller (eSDHC)

The Enhanced Secure Digital Host Controller provides an interface

for MMC, SD, and SDIO types of memory cards.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
1 回复
940 次查看
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Good references:

http://en.wikipedia.org/wiki/Secure_Digital

Freescale Enhanced Secure Digital Host Controller (eSDHC)

The Enhanced Secure Digital Host Controller provides an interface

for MMC, SD, and SDIO types of memory cards.

Regards,

David

0 项奖励
回复