I'm curious that MQX can support USB ULPI HS function.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm curious that MQX can support USB ULPI HS function.

1,661 Views
seongkeunjin
Contributor II


Hi everyone.

I'm developing a control platform using K60 kinetis device. And I have to use USB2.0 I/F which can support ULPI HS standard. Now I'm using MQX3.8.1 version RTOS. (I know it is lower version. But I have to use this version cause application compatibility.)

Anybody else who knows how to use USB ULPI HS I/F on MQX3.8.1?

Plz help me.

Thx.

0 Kudos
Reply
1 Reply

1,345 Views
soledad
NXP Employee
NXP Employee

Hello,

In MQX 3.8.1 the USB Host stack has been updated to be able to handle both Full Speed (EHCI) and High Speed (KHCI) modules simultaneously.

Please check the below thread:

Virtual Communication (COM) Demo - CDC device is necessary

I hope this helps, have a nice day!


Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply