I'm curious that MQX can support USB ULPI HS function.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm curious that MQX can support USB ULPI HS function.

1,662件の閲覧回数
seongkeunjin
Contributor II


Hi everyone.

I'm developing a control platform using K60 kinetis device. And I have to use USB2.0 I/F which can support ULPI HS standard. Now I'm using MQX3.8.1 version RTOS. (I know it is lower version. But I have to use this version cause application compatibility.)

Anybody else who knows how to use USB ULPI HS I/F on MQX3.8.1?

Plz help me.

Thx.

0 件の賞賛
返信
1 返信

1,346件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

In MQX 3.8.1 the USB Host stack has been updated to be able to handle both Full Speed (EHCI) and High Speed (KHCI) modules simultaneously.

Please check the below thread:

Virtual Communication (COM) Demo - CDC device is necessary

I hope this helps, have a nice day!


Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信