How to use the rtcs shell on ethernet instead of on a serial port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the rtcs shell on ethernet instead of on a serial port

跳至解决方案
1,066 次查看
jpderyck
Contributor II

The rtcs shell demo run on a serial port, how to run it on ethernet ?

It was possible on the security_telnet sample which was available with mqx version before 4.0,

I use the mqx 4.1 in wich this demo was removed

best regards

JP

标签 (1)
0 项奖励
回复
1 解答
905 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Paul,

The shell is targeted to work with the serial (CDC) interface. But you can also start a telnet session to take contro remotely of the Shell. Please take a look to the _README.txt file in C:\Freescale\Freescale_MQX_4_x\rtcs\examples\shell

Best regards,

Carlos

在原帖中查看解决方案

0 项奖励
回复
1 回复
906 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Paul,

The shell is targeted to work with the serial (CDC) interface. But you can also start a telnet session to take contro remotely of the Shell. Please take a look to the _README.txt file in C:\Freescale\Freescale_MQX_4_x\rtcs\examples\shell

Best regards,

Carlos

0 项奖励
回复